Industry Online Support
Technical Forum
10/31/2013 11:45 AM | |
Posts: 2930 Rating: (432)
|
Hi, no, the challenge is at your side. You need to solve it. |
This contribution was helpful to2 thankful Users |
11/2/2013 5:01 AM | |
Posts: 8 Rating: (0) |
This may be the idea ... but as I can improve ... so that between each action of the solenoid has a time of 3 seconds and at the end of the third solenoid, make a reseso for 8 hours and restart the sequence .... Attachment I made ... I'm sorry I'm learning .... AttachmentPURGA DE TANQUES.zip (188 Downloads) |
11/4/2013 6:24 AM | |
Posts: 8 Rating: (0) |
improved, with alarm and cycle control ..... if you can do more simplified. be welcome .... AttachmentPURGA DE TANQUES 2.zip (201 Downloads) |
Follow us on