3/6/2023 5:35 AM | |
Joined: 3/30/2020 Last visit: 3/19/2025 Posts: 5051 Rating:
|
The S7-1200 has the following CPUs: Most of these do not handle 5V. For that reason a signal board (200kHz) is available that handles 5V signals. It is still a secret, which one you are using. Consider then to verify the specifications of the CPU in the System Manual of the S7-1200 [LINK]. The appendix of the document carries the detail you need. |
Last edited by: qwazee at: 03/06/2023 05:37:23add link to system manual Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on