2/23/2017 2:35 PM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32921 Rating: (4069)
|
Here is a possible solution. You have the option to set the switch-on threshold for the heater using the cursor keys. But remember: you have to press the ESC key (ESC + Cursor key). Actual temperature less than 35.0 ° C, heater switched on. The actual temperature reaches 35.1 ° C and the heater switches off. If the actual temperature falls below 34.0 ° C (because of the hysteresis), the heater switches back on. AttachmentSetpoint adjustment via cursor buttons with limit_0BA8.Standard.zip (200 Downloads) |
2/23/2017 5:14 PM | |
Joined: 2/23/2017 Last visit: 2/18/2024 Posts: 37 Rating: (0) |
Thanks, I'll give it a try when I'm back in office. br Roger |
2/26/2017 9:28 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32921 Rating: (4069)
|
Hello flotul, you are welcome. |
2/26/2017 9:34 AM | |
Joined: 2/23/2017 Last visit: 2/18/2024 Posts: 37 Rating: (0) |
I'll give it a try too |
Follow us on