6/6/2013 9:18 PM | |
Joined: 10/9/2011 Last visit: 10/2/2024 Posts: 2 Rating: (0) |
Dear experts, I'm facing up to a challenge - how to convert special coded number into the simatic real format. The number contains two parts. The first one is a signed integer value (length 1 word) and the second one is display format (length 1 byte). This byte part's formed by another two nibbles (each length 4 bits). The high nibble (bits 4..7) indicates the number of decimal places and the low nibble (bits 0..3) indicates the total number of digits. Please see attached pdf file for better understanding. Is there any way how to convert this number into the simatic real format? Unfortunately I'm not able to find any easy way by myself. Any suggestions'll be really appreciated. Thanks in advace! Best regards PoliCZek AttachmentNumeric_form.pdf (160 Downloads) |
Follow us on