6/15/2011 10:49 AM | |
Posts: 35 Rating: (0) |
EXPLIQUER MOI D'OU PROVIENT LES 27648 ?
Attachmentconvesion valeurs analogique dans step7.zip (132 Downloads) |
6/15/2011 12:28 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Check the attachment to how convert raw converted digitized value(0 t0 27648) to the meanigful physical value in user program. Use of scale functionregards |
Last edited by: hdhosseini at: 6/15/2011 12:31 PM |
|
6/15/2011 1:28 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
EXPLIQUER MOI D'OU PROVIENT LES 27648 ?
Take a look at How 27648 Analaog Maximum Value ? Best regards, Hristo MIhalev |
6/15/2011 3:32 PM | |
Posts: 35 Rating: (0) |
MY QUESTION IS SIMPLE: what is the meaning of 27648 oterwise from where it comes.
Attachmentconvesion valeurs analogique dans step7.zip (73 Downloads) |
6/15/2011 3:37 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
For analog to digital conerter circuit inside the Ai card there is a hardware implementation to convert for example 0 to 4 mA to a digitized values.The hardware algorith maps 4 ma analog to 0 digital and 20mA analog to 27648.This value is set due to technical spec of manufacturer. Please note that the Digital to Analog converterinside AI convert this range of physical values to a WORD.In ALLEN BRADLEY controllers, the conversion is done from 0 t0 32767(0 t0 w#16#7FFF) and just one bit is reserved for error or sth(They also provide diagnostics data seperately).In HIMA as safety controller this conversion done from 0 to 700. For more information check chapter 4,5,6 of the following manual. SIMATIC S7-300 S7-300 Automation System Module Data regrads |
Last edited by: hdhosseini at: 6/15/2011 3:48 PM |
|
5/22/2012 2:03 PM | |
Joined: 5/1/2009 Last visit: 5/23/2021 Posts: 144 Rating: (1) |
Attachment14 Analog Value Processing.zip (107 Downloads) |
Best regard |
|
Follow us on