8/27/2022 3:31 AM | |
Joined: 1/7/2013 Last visit: 12/7/2022 Posts: 20 Rating:
|
Hello PCS7 V8.1 |
8/27/2022 11:25 AM | |
Joined: 1/11/2019 Last visit: 2/3/2023 Posts: 395 Rating:
|
Hello Eliyas, Select Blocks inside CFC chart > go to "Covert" >Select DW_BO single block or DW_W and W_BO block and interconnect them to convert Double Word data to Boolean . (See the attached for reference) DW_BO Block Function: This block converts the input value of the DWORD data type in 32 values of the BOOL data type, which are created at the 32 outputs. IN-Bit0 is then converted to OUT0, IN-Bit1 to OUT1 etc. DW_W Block Function: Copies the low-word of IN to the word of OUT. W_BO Block Function: This block converts the input value of the WORD data type in 16 values of the BOOL data type, which are created at the 16 outputs. IN-Bit0 is then converted to OUT0, IN-Bit1 to OUT1 etc. I hope, I have addressed your query! AttachmentConvert blocks.zip (53 Downloads) |
Follow us on