5/4/2016 6:08 PM | |
Joined: 11/21/2007 Last visit: 8/22/2023 Posts: 2321 Rating:
|
Hello Your question is not very clear. It seems you want to replace a Control desk with Hardware buttons with a Touch Panel with Soft Buttons. If your existing buttons are wired to a PLC and the PLC is controlling the whole system, then it is possible. You will then need to buy and configure a suitable HMI panel for your PLC type. It will also require some modifications in PLC software , to link soft buttons in place of hardware buttons. In case there is no existing PLC the of course you need to go in for a PLC + HMI. For this please contact your nearest Siemens Contact partner or Siemens Solution Provider. Retrofit & Modernization Services Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/5/2016 6:51 PM | |
Joined: 5/27/2012 Last visit: 8/17/2023 Posts: 177 Rating:
|
Thanks for helping. |
Follow us on