4/19/2010 12:39 AM | |
Posts: 15 Rating:
|
hello can anyone help me to convert s5 program to s7 program AttachmentZENTHEST.zip (1055 Downloads) |
4/19/2010 1:20 AM | |
Joined: 10/7/2005 Last visit: 7/11/2024 Posts: 3009 Rating:
|
Hellomhmmdhj Siemens can help you via theirSIMATIC S5-S7 Migration Support, you'll hopefully find the Technical Documents especially useful. I'd suggest you give itthe conversion a go yourself and use the Forum to ask more specific question should certain aspects of the conversiongive you problems. Please note too that you'll find plenty of FAQ's and Forum entries concerningS5 conversions, so starting with a search onhttps://support.automation.siemens.combefore postingmay speed up getting the answer to your questions. Last but not least,your S5 pogram is actuallya very simple one and has only 15 PB's (which always convert without problems), 1 FB and1 DBin use so it's a perfect "Beginners" program toconvert. I hope this helps and good luck. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
4/19/2010 10:19 PM | |
Posts: 15 Rating:
|
THANKS FRITZ THE PROBLEM I HAVE NO IDEA ABOUT SIMATIC S5 I DID NOT WORK WITH S5 BEFORE AND I TRY TO CONVERT IT AND I GET ERRORS AND WARNINGS |
4/20/2010 1:04 AM | |
Joined: 7/15/2008 Last visit: 1/23/2024 Posts: 382 Rating:
|
Hello mhmmdhj. Please see attached S7 Project with a 315-2DP. I also left the Source file in the Folder. In your S5 Program I deleded FB238 to FB251. ( not used ) If you use a PLC with a MMC Card you may not need to generate DB10 in OB101 Regards / m.f.g AttachmentZenthest.zip (692 Downloads) |
4/20/2010 9:55 AM | |
Posts: 15 Rating:
|
to legacy support thanks for your helping with my best regards |
6/9/2016 5:56 PM | |
Joined: 11/12/2011 Last visit: 7/11/2024 Posts: 2 Rating:
|
Hello sir (m f g), Can you also please help me to convert the attached S5 programme to S7 .. As i have tried so many times, but unfortunately encounter with many errors. and i really do not have any idea to rectify them. i will be very thankful to you for this. Regards Pradhumn AttachmentANSDK.zip (372 Downloads) |
This contribution was helpful to
1 thankful Users |
6/9/2016 9:30 PM | |
Joined: 11/12/2011 Last visit: 7/11/2024 Posts: 2 Rating:
|
Hello Sir, Please find the another attachment. For S5 to S7 conversion. I am not able to figure out which one is the right backup file. Please do the needful if possible. Thanks in advance Regards Pradhumn AttachmentSC0905ST.zip (400 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on