10/26/2013 3:19 PM | |
Posts: 34 Rating: (0) |
Hello please i want to convert OBs that contain STL program to LAD program ,with use Step 7 Professional? Regards |
10/26/2013 3:53 PM | |
Joined: 9/27/2006 Last visit: 5/22/2024 Posts: 12257 Rating: (2668) |
Hello, Abdul; Please, feel free to do so. I hope you understand that your post is incomplete, at least you could show us some of the code you want to convert. In any case, your machine understands very well the code in STL, it is much more efficient than LAD for the processor. I presume that you want to convert because you want to understand the STL code, but you will have to decipher it if you go through the conversion, and in that case it is better to comment the code thoroughly for review instead of converting to LAD or FBD. In any case, here is a manual on STL code, so you understand the basis of STL programming, and a FAQ discussing conversion issues that are prevalent when attempting a conversion, both from Siemens: SIMATIC STEP 7 V5.5 Statement List (STL) for S7-300 and S7-400 Programming Why can't you display an STL program in FBD or in LAD? AttachmentS7 STL to Ladder sample[1].pdf (1546 Downloads) |
This contribution was helpful to1 thankful Users |
5/10/2016 11:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by baal130 is split to a separate thread with the subject Code goes from lad to stl and was saved. Best regards |
1/18/2017 1:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by AutoGen_905449 is split to a separate thread with the subject How do convert TAK,BEC,XOD,INC STL code to LAD?. Best regards |
1/19/2017 11:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by hyo_eddie is split to a separate thread with the subject Instructional manual on how to program STL, SFC & IL in TIA portal?. Best regards |
Follow us on