3/12/2021 7:30 AM | |
Joined: 6/22/2017 Last visit: 3/27/2023 Posts: 344 Rating:
|
Hi Ant, i am not really sure, what is the best way to do so. It kind if depents how it should be connected to the rest of the Runtime. The cleanest way might be to build everything in Unified. It should also be possible to host this website aswell and use a Browser Control to show it during runtime. Technicly there is no real data connection regarding tags then. Third way would be to use your webpage as a custom web control. Reference: SIOS 109779176 I hope this gives you some ideas, what to do. Best regards, ZickZackTIA |
Follow us on