11/22/2016 11:35 AM | |
Posts: 6 Rating:
|
Dear All, I have a problem with Converting of STEP 5 assignment list to STEP 7 assignment list. For convert Step 5 project to step 7 project I use the next settings (see 1.jpg). The converting tool creates the next files (see 2.jpg): awl source, error file etc., but it does not create step 7 assignment list SA2110S7.SEQ at all. What do I do wrong? Attachmentscreen.zip (76 Downloads) |
11/22/2016 1:59 PM | |
Joined: 12/18/2014 Last visit: 11/28/2023 Posts: 31491 Rating:
|
Please upload the S5-files. |
11/22/2016 4:20 PM | |
Posts: 6 Rating:
|
Of course.AttachmentTEST.zip (48 Downloads) |
11/22/2016 5:00 PM | |
Joined: 12/18/2014 Last visit: 11/28/2023 Posts: 31491 Rating:
|
The problem is the different file names of the S5 files. The program file and the cross-reference list are named TEST1A *. *. However, you should also name TEST1A *. *, so that the symbol table for S7.SEQ can be created. AttachmentTest_2.zip (45 Downloads) |
This contribution was helpful to
1 thankful Users |
11/22/2016 5:32 PM | |
Joined: 1/21/2013 Last visit: 11/2/2023 Posts: 4617 Rating:
|
Hello, perhaps might help you: SIMATIC S5 to S7 Migration SIMATIC S5 to S7 Migration - Siemens |
11/23/2016 9:00 AM | |
Posts: 6 Rating:
|
Thanks for all. The problem is solved. |
Follow us on