Industry Online Support
Technical Forum
1/11/2013 4:53 PM | |
Posts: 74 Rating: (3)
|
Dear Engr Kashif I am not familiar with those model numbers and a search does not turn up anything. Do you have more info on the system andthe plugged chute detector? What is the technology, etc. Regard Toppie [ |:) |
1/14/2013 5:02 PM | |
Posts: 74 Rating: (3)
|
Hello Engr Kashif The part numbes and names you have provided are not familiar to me and I've been in this business with Siemens for over 25 years. What you describe uses either conductance or most likely capacitance. It's possible something like a CLS300 could be used but I don't know if that can be integrated into the existing system because I don't knwo the system. Another option would be a non contact system using (for example) the ULS200. This is commonly used for blocked chute detection Reference: ULS200 http://www.automation.siemens.com/w1/automation-technology-pointek-uls200-18707.htm CLS300 http://www.automation.siemens.com/w1/automation-technology-pointek-cls300-18698.htm Photos or a sketch could be helpful. Regards, Toppie [ |:) |
Follow us on