4/5/2017 12:52 PM | |
Joined: 9/23/2005 Last visit: 5/23/2024 Posts: 4552 Rating: (699) |
Overlay (with AT operator) the array of BOOLs with an array of DINTs. You may find this helpful. |
Last edited by: jacek d at: 4/5/2017 1:03:25 PMRegards, |
|
4/5/2017 1:08 PM | |
Joined: 9/16/2010 Last visit: 4/30/2024 Posts: 109 Rating: (9) |
Or you copy the Array of bool with GATHER / GATHER_BLK into DINT / Array of DINT. This are new commands in V14 SP1 |
4/5/2017 5:38 PM | |
Joined: 9/16/2010 Last visit: 4/30/2024 Posts: 109 Rating: (9) |
And here the overlay variant.
See the attchment for an FB-source, writen for FW2.2. errDWordArr is overlaying errBoolArray. This works in FB's with set remanenz in idb. AttachmentCheckErrBit.scl.txt (669 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on