7/18/2012 11:33 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello, there are some FAQs in the internet and I hope these could be meanful for your: http://support.automation.siemens.com/WW/view/de/59623719 http://support.automation.siemens.com/WW/view/de/57132240 http://support.automation.siemens.com/WW/view/de/42603881 With best regards |
7/18/2012 2:41 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2376)
|
Unfortunately trying to perform a block copy from the input image is not an 'array' operation, so these FAQs are not helpful. For now, I manually typed all the move commands referencing all the input words one word per move command, and manually indexing the destination array. I know in legacy Step 7 this is fairly easy to do. The portal still has a ways to go even after the recently released V11 SP2 Update 4. |
science guy |
|
Follow us on