7/4/2014 11:53 PM | |
Posts: 5225 Rating: (1185) |
Hi there. What do you mean when you say "LS"? Are you talking of a PLC brand? What card is mentioned.. SD card or cartrage type. Mentioning the part number of the LOGO! might also help a little. Maybe a photo of the PLC with card can help us, help you. Please find attached an extract from the System Manual. Please see if this helps you. But do get back to us with some feedback. Good luck. AttachmentEXTRACT_LOGO System_manual_Security function.pdf (211 Downloads) |
7/5/2014 9:29 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello William B. Maybe our friend EPKKN speaks of this in Fig.05 but for LS I do not know, let's see if it will give us more information memory/battery cards can be used with which LOGO! - Siemens ... |
This contribution was helpful to1 thankful Users |
Follow us on