4/22/2024 1:20 AM | |
Posts: 1 Rating:
|
Hello! Why is it so, how to fix it? LSC 8.4 is installed. I open the program created back in LSC8.3, but modified and resaved in LSC 8.4 and the copy-paste blocks are working fine, and the following lines appear in the info window: *** 4/22/24, 2:59 AM LOGO! 8.3_1 Diagram *** *** *** *** *** *** *** *** Paste from clipboard (Only texts can be copied) Blocks with changed properties: M1 [Flag]: M17 --> M1 B001 [NOT]: B006 --> B001 In the other one, created in LSC 8.4, the copy-paste does not work, although I copy the same thing. In info it writes: *** 4/22/24, 3:01 AM LOGO! 8.3_1 Diagram.lsc *** Paste from clipboard (Only texts can be copied) Also if I make a cut, then I can say goodbye to the blocks. |
Last edited by: Jen_Moderator at: 04/22/2024 11:24:42Text formatting optimized. |
|
4/22/2024 1:49 AM | |
Joined: 12/18/2014 Last visit: 4/18/2025 Posts: 35133 Rating:
|
Start a Support Request. |
1/5/2025 2:35 PM | |
Joined: 12/20/2024 Last visit: 4/17/2025 Posts: 1 Rating:
|
Is there already a solution for this problem. Got the same message and outcome. Thanks in advance. Regards, Ed |
1/5/2025 5:03 PM | |
Joined: 12/18/2014 Last visit: 4/18/2025 Posts: 35133 Rating:
|
Install the current version V8.4.1 of LSC. You can download the upgrade to LSC V8.4.1 from here: Firmware update for LOGO! 8.4 basic devices and service pack 1 for LOGO! Soft Comfort V8.4 |
We are working on a new user interface with better overview and more relevance.
Follow us on