4/16/2023 10:42 PM | |
Joined: 3/28/2010 Last visit: 7/14/2024 Posts: 1049 Rating:
|
1. Response of Coriolis technology Check the graph on the far left, "Nominal Step Response" You can see that the Coriolis was the slowest responding of the four technologies, and by extrapolation you can see that the response to a square change at the input was still only 2 seconds, not 30 minutes. So I agree that if your density is constant, 30 minutes is an unreasonable response for density measurement. Here's the paper's comments on Meter Zero: |
Follow us on