Industry Online Support
Technical Forum
4/16/2012 6:56 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Take a look atWhat should you watch out for when using the RS485 repeater in PROFIBUS and MPI bus systems?in order to check distance and baud rate. Using the manual from that FAQ you can see what is the right way for connceting cable and connector. If for some reason copper profibus cable is not 'suitable' - use FO. Best regards, Hristo Mihalev
|
4/16/2012 11:59 PM | |
Posts: 5 Rating:
|
Hi Umencho, no problem because the conection is in 187,5Kbytes/s, with 300meters there is not problem. |
4/17/2012 1:19 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed in the following thread Problems with communications. Equipment damage or fail Best regards O_Moderator |
Follow us on