Industry Online Support
Technical Forum
1/21/2011 10:56 PM | |
Posts: 8 Rating: (0) |
hi guys! Im trying to get a correct sequence of the outputs. what i want is to turn output1 on when it goes below a certain level and to turn back off when it reaches the specified level. when the output1 is on the output2 should stay off until it reaches the specified level to come on. atthis moment both outputs 1and2 should be on and they should go off when getto the specified point. the main thing that i am struggling with is thatwhen output1 comes on so deos the other one. can anyone please let me know what is rong with the code??? thank you very much in advance! Attachmentsequence.zip (306 Downloads) |
1/22/2011 8:21 AM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
take a look at the attachment maybe it help you also when you upload dont rename the file ,but create a zip file your attachment is a renamed ( .lsc > .zip ) and maybe some members of the forum will not be able to open and help you best regards Attachmentsequence1.zip (312 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
1/22/2011 10:43 PM | |
Posts: 8 Rating: (0) |
you are a STAR!! thanks ever so much!! i do appreciate it man! |
Follow us on