11/11/2020 1:02 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
Hi, it is not included for Tel352 -> so download the library from here and open it in TIA: https://support.industry.siemens.com/cs/de/en/view/109747655 (see LSinaExt in bottom of the page - it includes a block for tel352 and one for tel20). Please note that the blocks as they are only work if you have configured the telegram exactly without any extension. Otherwise you need to adapt the block which of course is also possible as it is open. |
Best regards, |
|
Follow us on