11/27/2018 12:55 PM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hi, I am curious: Will the first client work if the server is not upgraded yet? (Could I use WinCC 7.4 SP1 for the client with a server running WinCC 7.0 SP3?) Will the updated programs keep on running correctly even though the licenses are for an older version? Why not start by updating the licenses - they should all be backwards compatible - or not? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/28/2018 8:35:19 AMNew subject after splitting |
|
Follow us on