8/8/2023 8:17 PM | |
Joined: 10/15/2022 Last visit: 7/6/2024 Posts: 66 Rating:
|
Hi, LOGO! enthusiasts! Another demo from me, this one introduces options for limiting counter values. There are three counters in the program and they behave differently when the limit is reached or exceeded. I got the logic of the second counter from an German speaking forum and adjusted it a little (see also "LOGO! - Software" area, topic "Counter input limiting?") Important to know! When simulating program, counter start value not changing automatically. Tested on the real controller (6ED1052-1MD08-0BA1, with firmware 1.83.02) several times. Three files in the zip file (program, scheme and description). Andrus AttachmentCounter limit demo.zip (426 Downloads) |
Last edited by: Andrus_Saar at: 08/08/2023 20:24:13Last edited by: Andrus_Saar at: 08/08/2023 20:46:32Last edited by: Andrus_Saar at: 08/08/2023 20:53:13Last edited by: Andrus_Saar at: 08/09/2023 05:53:38 |
|
This contribution was helpful to
1 thankful Users |
Follow us on