12/12/2019 11:00 PM | |
Joined: 9/21/2012 Last visit: 4/28/2024 Posts: 3930 Rating: (444) |
There is a IE/PB Link PN IO for Profinet<->Profibus communication. |
12/12/2019 11:16 PM | |
Joined: 9/27/2006 Last visit: 4/28/2024 Posts: 12257 Rating: (2665) |
Hello Urantia; Siemens has developed PN/PN Couplers, as well as DP/DP Couplers. Ses the attachment below. As per the PN/PN Coupler manual, https://support.industry.siemens.com/cs/us/en/view/44319532 you can configure the coupler directly in TIA Portal, on one side. And use the gsd file to integrate it in any other control program, including Simatic Manager. Since each "side" of a coupler is configured in its client (master) controller, it is of no importance what software is used on each side. What is important is that the configuration matches on each side, as defined in the manual. Hope this helps. |
Last edited by: dchartier at: 12/13/2019 00:53:35 |
|
12/14/2019 1:49 AM | |
Joined: 9/27/2006 Last visit: 4/28/2024 Posts: 12257 Rating: (2665) |
Hello Urantia; Sorry that I misunderstood your requirement. If that is the case, Hati's suggestion of an IE/PB Link should be a possible solution to your problem. Open the link in his post, for initial information. Look up the operating instructions manual here: https://support.industry.siemens.com/cs/us/en/view/109745581 Daniel Chartier |
Last edited by: dchartier at: 12/14/2019 12:06:48 |
|
12/18/2019 2:53 AM | |
Joined: 10/23/2009 Last visit: 3/11/2024 Posts: 114 Rating: (0) |
Dear Haiti, Dear dchartier. Thanks for your support. I will try the solution that your mention. Best Regards! |
Follow us on