3/7/2019 10:44 AM | |
Joined: 4/25/2017 Last visit: 4/15/2025 Posts: 436 Rating:
|
Hi, Please check this example: S7-based Telecontrol via DNP3 Protocol In Chapter 7.3 is a step for step description for setting WinCC as DNP3-Master. You have to create a "DNPCONN" and a "DNPRTU" Node. Regards, Kirschiaub08 |
Best Regards, |
|
This contribution was helpful to
1 thankful Users |
3/7/2019 4:53 PM | |
Posts: 52 Rating:
|
I have actually followed the manual step by step and did create the nodes, but unfortunately the tag properties in WinCC 7.4, in the section for "Address" it is still empty for the Telecontrol tags, as shown in the photo attached.
|
Last edited by: ASIMO99 at: 3/7/2019 4:54:55 PM |
|
3/8/2019 8:27 AM | |
Joined: 4/25/2017 Last visit: 4/15/2025 Posts: 436 Rating:
|
Hi, If you are using WinCC V7.4 SP1 you need to install a Patch: SIMATIC WinCC TeleControl V7.4 compatibility with SIMATIC WinCC V7.4 SP1 Best Regards, |
Best Regards, |
|
3/12/2019 3:09 PM | |
Posts: 52 Rating:
|
Thank you for your reply. I downloaded and fixed the patch, but unfortunately the tag address section is still the same (empty) :) |
3/27/2020 6:54 PM | |
Joined: 9/2/2012 Last visit: 3/28/2025 Posts: 711 Rating:
|
Dear ASIMO99, Is your problem solved ? If so kindly share the solution, am also facing the same issue. for other - 1. I have s7 300 with TIM 4R-IE is the configuration, step7 v5.6; Sinaut ST7 configuration-v5.5 sp3 2. WinCC v7.4 sp1 update 8 3. Telecontrol Server Engineering + Telecontrol Server Runtime + DNP3 License are available.-> V7.4 Setting attached herewith. AttachmentSETTINGS TC.zip (165 Downloads) |
|
|
3/28/2020 7:22 AM | |
Joined: 9/2/2012 Last visit: 3/28/2025 Posts: 711 Rating:
|
Update- Updated the channel driver with Patch file given in the link, but no success. |
|
|
Follow us on