10/9/2013 2:02 PM | |
Posts: 567 Rating: (107) |
Hi, CP1613 A2 is compatible with Microsoft Windows Server 2008 R2. CP 1613 is not compatible. You can find this information under the following link on page 16: http://support.automation.siemens.com/WW/view/en/66807356/0/en |
This contribution was helpful to1 thankful Users |
10/10/2013 7:28 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
Hey, i hope the following FAQ clears your question: http://support.automation.siemens.com/WW/view/de/23785421 The CP1613 is NOT compatible with Windows Server 2008 R2 64bit, the CP1613A2 is compatible. |
Best Regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on