Industry Online Support
Technical Forum
6/9/2007 4:08 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Kolma, When you open a project then there are "Projects", "Examples", "Librarys" and "Multi Projects" that you can open. The project you mentioned must be placed in the "Examples" - TAB. When the example is not there then you maybe not installed the PtP option package.... You can download this on the next link Download CD "CP340, CP341, CP440, CP441", version: V5.1+SP7. Please also check if the newest blocks are used in the example. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/8/2009 10:02 AM | |
Posts: 8 Rating:
|
Hi Late, I also need this sample. I follow your link but not any document/project here. Please help me more...Thanks! BR, AnUyen |
1/8/2009 10:59 PM | |
Posts: 63 Rating:
|
Corrected link: Software and Documentation version 5.1 + SP9 |
Follow us on