7/12/2011 2:50 AM | |
Joined: 10/7/2005 Last visit: 4/29/2025 Posts: 3047 Rating:
|
Hello maktas to start with, status code 8180(hex) means "There is no data available yet". Without looking at your code and configuration, I could only speculate as to the reason for this (e.g. lenght does not match, incorrect connection configuration etc.), so allow me to point you to some additional resources in which you will hopefullyfind the answers: How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? What properties, advantages and special features does the UDP protocol offer? How do you send/receive data to/from multiple communication partners via the IE CP of an S7-300 or S7-400 station using the UDP protocol? Functions (FC) and function blocks (FB) for SIMATIC NET S7 CPs Programming Manual I hope this helps and please let us know what you find out. |
Cheers |
|
Follow us on