Industry Online Support
Technical Forum
11/3/2011 10:06 AM | |
Joined: 9/22/2010 Last visit: 7/25/2024 Posts: 225 Rating: (28) |
You can only use the Modbus TCP Wizard with a CPU with an integrated PN interface. When using a standard CPU and a CP343-1 you have to do the configuration of the Modbus block manually. In general you can download the MODBUSCP block at www.siemens.com/s7modbus(ModbusTCP CP V4.3). After installing it you can find a manual, a library and an example project. Regards Sakura |
Last edited by: Sakura at: 11/3/2011 10:07 AM |
|
11/3/2011 10:19 AM | |
Posts: 15 Rating: (0) |
Ok, thank you Sakura and Kaulquappe for this help. |
Follow us on