Industry Online Support
Technical Forum
8/23/2022 2:58 PM | |
Joined: 1/10/2022 Last visit: 12/13/2023 Posts: 20 Rating:
|
Dear all, I'm using CP 1243-7 LTE module, While I'm inserting the sim card in the cp card it Diag led blink in Red and the Network glow red steady but now the CP card showing that there is a no sim card inserted (as per the cp 1243-7 lte manual). I don't know why this is happened but the in one station the Telecontrol server connection has been established and there was no these types of error i have faced , but the sim card is also has the network , range and i have changed the sim card which has been used in the first station which is working perfectly. But in the working station while I insert the sim card if is it in a TCSB connection or not in a TCSB connected the network glows in green and Diag blinks green. But in other 2 stations only I face these issue, please say if i miss any configuration for the TCSB connection. Kindly please give a solution for my problem..... Regards, Kiruba Robert ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/24/2022 10:16:46New subject after splitting Kiruba Robert |
|
Follow us on