12/8/2012 8:08 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi All, I have installed new CP1613 A2 on OS machine IPC 547C. Now I have two problems:
Now question is will I be able to use CP1613 for AS-OS communication over ISO given the above two problems? I gave a try to this but didn’t succeeded so I want to be sure that it is technically possible. Meanwhile under device manager it does not show any error in CP (shown in picture “device_manager.jpg” and “driver.jpg”). Also attached is the picture showing list of installed software with their versions on OS (“versions.jpg”) for reference. Iam using PCS7 V6.1 SP3 and OS is Windows Server 2003 R2 SP2. Thanks for your time, Regards Manmeet. AttachmentCP1613.zip (139 Downloads) |
12/13/2012 9:44 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi Thanks JOTST and Rated X. Everthing is up and working. Intially I just reaplced CP1623 in IPC with that of CP1613, all this with PCS7 installed. But as mentioned inmanualsection 2.2, I did fresh install (recovery dvd) of OS, followed with fresh PCS7 installation. Things started falling in place after this. Also intially I was under impression that NDIS is a must for CP1613 to work, but now I know its not (Thanks to JOTST).NDIS is only needed when you want to use CP1613 for networking purpose. Regards, Manmeet.
|
Follow us on