Industry Online Support
Technical Forum
11/26/2013 7:23 AM | |
Posts: 25 Rating:
|
I have got 1 no. CP 1613 & 1no. CP 1623. Can these two be used in a PC? Redundancy can beestablishedwith these two cards? |
11/26/2013 9:58 AM | |
Posts: 1368 Rating:
|
Hello NBRM, according to your first question: You can install max. 4pieces ofCP 1613/CP 1623 in your PG at the same time. Which kind of redundancy do you want to realize? With the SIMATIC NET SOFTNET-IE RNA V12 you can establish a redundant network based on PRP. http://support.automation.siemens.com/WW/view/de/74082758 Regards, Pittiplatsch |
11/26/2013 10:16 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Check also hardware and software compatibility for both cards. |
Follow us on