Industry Online Support
Technical Forum
5/18/2016 11:26 PM | |
Joined: 2/5/2016 Last visit: 6/28/2022 Posts: 20 Rating: (0) |
I have configured for the CP1613 IP address and MAC address at the same time and then I download it to the Workstation, but it give an error and stop . it works only when I use the MAC only,is there a method to configure the IP and MAC at the same time and work? AttachmentCP1613 ERROR.pdf (55 Downloads) |
Follow us on