5/20/2016 6:33 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi Sowma, You can only work with fault tolerant connections on the ISO protocol...it does not work on TCP/IP. Below is made clear when you use ISO (MAC) and when you use TCP/IP: Normally plant bus communication is through ISO protocol, but you can use TCP/IP under the following conditions:
Use the ISO protocol under the following conditions:
|
Last edited by: Oreca at: 5/20/2016 7:16:55 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on