4/29/2013 11:50 AM | |
Joined: 3/19/2012 Last visit: 11/10/2022 Posts: 18 Rating: (1) |
Conzerv energy meter EM6400 series are communicating but the result is sluggish. There are 18 numbers of meters connected as shown in the attached file 'EM6400 wiring'. Customer used profibus cable to take all the meters in loop. CP341 is used as modbus master. Software used is PCS7 v8.0 update 1, CPU 416-5-H PN/DP. Necessary driver and license were installed. The baud rate is 9600, parity even and stop bit 1. Unique slave addresses are assigned to the respective meters. S7HMODM3 block, EXSQ_MOD bock and MODMR_R blocks are used for reading holding registers from the meter. The problem I am facing is the slow communication and very intermittent when communicating with all the slaves. Various problems are been faced which I have mentioned in a word file as found in the zip folder. AttachmentModbus Issue.zip (314 Downloads) |
4/30/2013 8:47 AM | |
Joined: 3/19/2012 Last visit: 11/10/2022 Posts: 18 Rating: (1) |
Hi Manmeet, In the maual(as attached) for the library says that S7HMODM3 and MODR_R can be used in a different OB's. The meters were wired as per the EM6400 manual. Firstly I had connected only one meter and kept the meter in the simulation mode and I was reading upto 20Registers in one query.Later when I switched the meter in RUN mode I was not able to read more then 6 registers also the response was slower. While reading multipe slaves and requesting different slaves in next query the reponce was very sluggish.Thedrivers loaded in CP341are proper and they match with the set parameters in the Meter. AttachmentPCS7_S7HMODM3_v3.0_E.pdf (366 Downloads) |
8/22/2013 5:07 PM | |
Posts: 3093 Rating: (323)
|
Hello Ravi, you can change the scan time for OB35 etc. in the properties of the CPU. Regards, Kaulquappe |
8/22/2013 5:39 PM | |
Posts: 247 Rating: (2) |
Dear Kaulquappe, Thank you, i appreciate if you provide any link or screen shot for doing the same. Regards, RaviS |
7/24/2017 1:47 PM | |
Joined: 6/19/2017 Last visit: 5/21/2024 Posts: 8042 Rating: (164) |
New question published by HarePrasath is split to a separate thread with the subject Where is S7HMODM3 library for RS485 communication using PCS7?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on