Industry Online Support
Technical Forum
9/23/2014 9:34 AM | |
Joined: 6/26/2013 Last visit: 4/23/2024 Posts: 143 Rating: (5) |
Dear all, I have to communicate CP341 RS232(C) with a non siemens plc. Should i make a cable with the S7-S7 configuration (http://support.automation.siemens.com/WW/llisapi.dll/csfetch/218300/CpS7_CpS7_e.gif?func=cslib.csFetch&nodeid=26588045) or just use RxD, TxD and GND pins? Regards |
meeda_ |
|
9/23/2014 12:43 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307)
|
Hello meeda Pl check the manual of your communications partner for the pin details of the same. Usually however if it has a 9 pin RS232 port, the pin details should be same ( But I have seen many non siemens hardware with non standard pin configuration ) Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on