12/8/2008 4:53 PM | |
Posts: 2 Rating:
|
Dear sir, I have a configuration with CPU313C, CP 342-5 (as a DP Master) and with modular DP slave. Each DP slave has two I/O modules (first with 4 words and second with 6 words), please see atached file. Is it possible to receive data separately from each module i.e. FC2 for receiving 8 bytes (from first I/O module) in some DB location and FC2 for receiving 12 bytes (from second I/O module) in some another DB location (two times call FC2, first call FC2)? If I try I get message: Inupt data lenght: DP_RECEIVE 8 (12) bytes is too short. The configured arrea is 20 bytes. What in case if I have configuration with 5 DP slaves like this? Does it mean that the CPU automaticaly configures data lenght for communication (in this case 100 bytes)? thanks in advance AttachmentDoc1.pdf (225 Downloads) |
Last edited by: CS Moderator at: 12/8/2008 11:51 PMnew subject after splitting |
|
12/9/2008 6:53 AM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello miki161, J_Bell is right. Just to confirm his explainations with pictures: See this FAQ: Processing the data from DP slaves via CP342-5 on CPU31x regards |
12/9/2008 7:59 AM | |
Posts: 2 Rating:
|
Thank You sirs! best regards |
Follow us on