2/6/2008 1:42 PM | ||||||||||||||||||||
Joined: 10/12/2006 Last visit: 9/30/2024 Posts: 206 Rating: (25) |
Hi Erik, No I think the problem not this, because:
Can you ping your cp343 ? if not maybe the configuration isnt there. becouse when you download the hw config to the cpu, the step7 give a popup window, and this window you can select the cpu, and the cp card. If you select the cp the step7 download the datas to the ethernet card. Regards Zenta |
|||||||||||||||||||
2/6/2008 1:56 PM | |
Posts: 3 Rating: (0) |
Hi. I can ping the CP from my panel and from my PC. I have connected them through a switch. - Eirik |
2/6/2008 2:25 PM | |
Posts: 3 Rating: (0) |
Problem solved. The rack/slot was set to 0/4, wheras on a S7-300 it is always 0/2. - Eirik |
2/6/2008 2:34 PM | |
Joined: 10/12/2006 Last visit: 9/30/2024 Posts: 206 Rating: (25) |
Ok. Zenta |
Follow us on