6/3/2011 3:27 PM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating: (1053)
|
Hello DaveA any real I/O conflict would have been detected by the compilation of the HWconfig, so I wonder if you have the problem as described in the link below (if so follow its remedies and/or update the firmware of your 315): What do you have to do if the SIMATIC S7-300 CPU no longer goes into RUN mode after adding a CP or FM module? I hope this helps |
Cheers |
|
6/3/2011 3:35 PM | |
Posts: 691 Rating: (36) |
Can you post your diagnostics buffer and Hardware configuration as asked by Ammy Is there any address conflict btween the PLC System and your PC MPI/Ethernet |
6/4/2011 2:26 PM | |
Joined: 8/8/2008 Last visit: 7/4/2024 Posts: 78 Rating: (4) |
I must admit I have never updated the firmware of a CPU before. What are the basic events that take place / what is required i.e do I have to download the program, will the CPU loose and data etc? Thanks for the replies! :-) just looking at this, I was wondering if it is possible to find out which firmware is currently in the cpu?
|
Last edited by: DaveA at: 6/4/2011 2:48 PM |
|
6/4/2011 2:35 PM | |
Joined: 8/8/2008 Last visit: 7/4/2024 Posts: 78 Rating: (4) |
Please see attached on the messages given in the diagnostic buffer...... |
6/4/2011 2:49 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, In order to update the firmware follow http://support.automation.siemens.com/WW/view/en/16750732. There is need a bigger MMC card...
No, I don't think so. Did you try SaravanaKumar suggestion? Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 6/4/2011 2:58 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on