11/14/2006 4:36 PM | |
Joined: 4/24/2006 Last visit: 8/27/2024 Posts: 8724 Rating: (1166) |
Hello, I think you should upgrade your Step7 to v5.4 See following link: http://support.automation.siemens.com/WW/view/en/23868313 Best regards, Wizard |
11/15/2006 1:55 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Dear RaGud, It depends on what kind of feature you want to use. If you want to use the PN IO Device functionality you need at least Step 7 v5.4 with HSP 1011 or Step 7 v5.4 with SP1. With HSP1011 you can also use the following 2 links: Download GSDML File for CP 343-1 Lean (6GK7343-1CX10-0XE0) Download: New STEP 7 Online Help System for CP 343-1 Lean If you want the othere IE functions you need atleast v5.3 and SP1. |
Best regards, |
|
Follow us on