9/18/2013 4:34 PM | |
Posts: 1 Rating:
|
I've recently updated Step7 5.4 SP4 with new Hardware Config andupdateda standard program with a newer CPU314 from 6ES7314-1AG13-0AB0 to 6ES7314-1AG14-0AB0. Since thenI have been having problems trying to get CP343-1 (6GK7343-1CX00-0XEO) to work. I have attached CPU314 module diagnostic report. I have read simular issues relating to HW config of the CP343-1 (firmware V3.0) using SP5 Hotfix 5 & 8. Would this be the cause? I even triedan older firmware on the CPU314 from V3.3.8 down to V3.0.3 as it said it required Step7 5.5 but I only got rid of one error. The CP343-1 is currently V3.0 firmware The two errors are: Parameter assignment error assigning parameters to modules (not on P bus, cancel download) no relevance for user: SDB number: 1004 no relevance for user: SDB number: 1003 no relevance for user: SDB number: 1001 AttachmentDiag.zip (113 Downloads) |
Last edited by: O_Moderator at: 9/19/2013 7:34 AMattachment reattached |
|
10/2/2014 9:04 AM | |
Posts: 8 Rating:
|
Hi, I have exactly the same problem. Have you fixed it ?
|
Follow us on