12/3/2008 9:04 AM | |
Posts: 3 Rating: (0) |
Hi J_Bell ....... Irvine and I are trying to establish a communication to our respective PLCs. On my side, I have a redundant S7-400 system using CP443-1 for communication. On the NETPro, I configured my side of the station as shown on JPEG files "NetPro Config 001 & 002". The station configuration for the S7-300 station (Irvine's side) is as shown on the JPEG files "NetPro Config 003". CP443-1 <--> Router (172.16.16.1) <--> NTU ---- NTU <------> Router (172.20.1.1) <--> CP343-1 | CP443-1 <- We are trying to use BSEND and BRECV to transfer data blocks. While using S7 NCM "PING" option, we tried to ping to each other's CP.We kept getting a No Response Thanks in advance!!! AttachmentNetPro Config.zip (217 Downloads) |
12/9/2008 1:31 AM | |
Posts: 15 Rating: (0) |
Hi J_Bell, Thanks for the informations, we finally got communication link across. Best Regards, Irvin |
12/9/2008 12:02 PM | |
Posts: 5822 Rating: (412)
|
Hello Irvin, thank you for telling. I hope my hints could help you solving your situation. Best regards J_Bell |
Follow us on