12/29/2014 7:01 PM | |
Joined: 5/13/2013 Last visit: 4/7/2023 Posts: 1 Rating: (0) |
I am working on PCS-7 V8.0 ,in my HW configuration I have CP-443-1,how many ways are available to communication with third party and which protocol ------------ New subject after splitting from cp443-1. |
Last edited by: Min_Moderator at: 12/30/2014 1:56 PMSplitted |
|
12/29/2014 8:05 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello Rajiv; For a list of supported protocols on the CP 443-1, open the following link: What differences are there between the Industrial Ethernet CPs of SIMATIC S7-400? The attached file shows which protocols are supported by different variuations of the CP 443-1. The list does not include "external" software blocks, such as this Open Modbus/TCP offering from Siemens IT4Industry: Open MODBUS/TCP for SIMATIC systems - Siemens And look at the links provided earlier by Hamid Hosseini. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/30/2014 12:28 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on