7/6/2013 12:18 PM | |
Joined: 1/20/2008 Last visit: 10/8/2024 Posts: 120 Rating: (7) |
Hello cucoo, You can configure it directly by HW Config in Simatic Manager same as CPU or SM cards. If you can't find CP's order code in HW config, please install lasted hardware updates. Also, for firmware update, take a look to at this link. |
7/11/2013 7:49 AM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Check this: Modbus to TCP/IP Communication with CP443-1Update if it is not your case. |
Last edited by: hdhosseini at: 7/11/2013 7:50 AM |
|
7/11/2013 8:07 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Have a look at this FAQ. How do you configure an ISO transport connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced? Hope this helps. |
Last edited by: Amit_86 at: 7/11/2013 8:12 AMLink Added VANDE MATARAM..... |
|
7/11/2013 8:24 AM | |
Posts: 20 Rating: (0) |
sir im not getting full information from that link.can you please tell me which all are the FB's i have to use for that cp443-1 configuration in my program |
7/11/2013 8:27 AM | |
Posts: 20 Rating: (0) |
thanks sir |
7/11/2013 9:04 AM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Hello, If your DCS side supports MODBUS like the general DCS options,You can try:
Hamid Hosseini |
Follow us on