9/3/2008 7:46 AM | |
Joined: 9/28/2005 Last visit: 12/10/2024 Posts: 2957 Rating: (243) |
Hi, I think you forgot to attach diagnostic file |
Best regards, |
|
9/3/2008 8:52 AM | |
Posts: 7 Rating: (0) |
Sorry, the txt file was blocked.
AttachmentCP443-5Ext_Diagnose.zip (478 Downloads) |
9/3/2008 11:13 AM | |
Posts: 7 Rating: (0) |
OK, I will ask customer for details. Thank you! |
9/12/2008 4:57 AM | |
Posts: 7 Rating: (0) |
Hello, J_Bell, Here is some more info: The system started on Apr. 2007. This error happens since that time.In this few months, the error happens more frequently. The CP443-5 DP line is only used for master/slave comm. No PG/OP connected on this bus. The bus is in line structure, and the total lenght of the bus is about 50 m. They also sent me the hw config file, please see the attachment. Thanks a lot! Attachment20080905.zip (415 Downloads) |
Follow us on