Industry Online Support
Technical Forum
6/5/2010 2:12 PM | |
Joined: 8/25/2006 Last visit: 10/18/2024 Posts: 2209 Rating: (279) |
Hello! Flashing 0 means initialisation error. So you should read the module information to understand the reason of this error. May be you have not configure something else in your program which may cause such error. D7-SYS V6.2 is sufficient for working with CP51M1 V1.1.2. Which FW version now has your CP51M1? If you will use D7-SYS V7.0 please read the following restrictions. But you need not upgrade your D7-SYS version, CP51M1 will work ok with V6.2 SP3. |
This contribution was helpful to1 thankful Users |
Follow us on