9/20/2017 2:10 PM | |
Posts: 7 Rating:
|
Hi all, i have CP5622 in my computer with BMS system. All worked, but once Windows 7 (64 bit SP1) install updates and then i had problem like this https://support.industry.siemens.com/tf/ww/en/posts/cp-5612-internal-error-in-a-pc677b/141475/?page=0&pageSize=10 . Unistalling updates didn't help, replacing card also, i even reinstall soft Simatic NET (card wasn't at computer) and now i just have Unkown device = network controller in the list of other devices. Neither online installing driver nor installing from CD SIMATIC NET doesn't work. I also reinstall Net.Framework and nothing... what i can try more? |
9/25/2017 12:06 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello Gusha123 perhaps this FAQ can help you, I used it also a few times with success: http://support.automation.siemens.com/WW/view/en/11870489 ByeMurof |
If this Information really helps, you could use the Rate function |
|
11/9/2017 9:49 AM | |
Posts: 7 Rating:
|
In the end helped only reinstaling Windows and SIAMTIC NET. |
This contribution was helpful to
1 thankful Users |
Follow us on