5/4/2016 12:50 AM | |
Posts: 2 Rating: (0) |
Hi.... I have same problem too. My PLC is S7-1200 , CPU 1212C , AC/DC/RLY , my software is TIA V13. i can not download program to PLC and go to online mode. i can not configure hardware. i see the PLC in software without connection whit PC. what can i do? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/4/2016 11:45:58 AMNew subject after splitting |
|
5/4/2016 7:30 PM | |
Posts: 2 Rating: (0) |
Hi... i can not attach pictures here but i send you links of pictuers -delete links, add Attachement- Attachmentpictures.zip (177 Downloads) |
Last edited by: industry support at: 5/4/2016 7:37:36 PMLast edited by: Min_Moderator at: 5/6/2016 2:17:55 PMAdd attachment |
|
5/5/2016 8:30 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, can you pls post info about your OS, TIA has some SP or update? |
With best regards... |
|
5/13/2016 9:53 AM | |
Posts: 1 Rating: (0) |
me too, hi you! are you fixed error ? you can help me fix it pls. thank you :) |
5/13/2016 1:57 PM | |
Posts: 310 Rating: (18) |
Hello, First You have to set PC-IP Address . Corresponding to PLC . Like 192.168.0.10.. ( Last Digit Is different From your Network Used).. After That u have to Check Your Device Name Of PLC Setting .. Regards, Arasan.. |
Follow us on