2/14/2013 12:31 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, Your sensor is a 2 wire sensor (datasheet), did you connect it as shown in: How do you connect a sensor to the analog signal modules of SIMATIC S7-1200? The first analog input is IW 112. After that another problem: the sensor is 4-20 mA, the analog input is 0-20 mA. In STEP 7 (TIA Portal) V11, how can you scale integer values in real numbers and real values in integer numbers for analog measurements? Regards, Marcjan |
Last edited by: Marcjan at: 2/14/2013 12:35 PMProblem solved? |
|
2/15/2013 7:26 PM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
HellowMarcjan Thank you so much. got it done |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
This contribution was helpful to1 thankful Users |
3/26/2018 10:15 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by tvr126 is split to a separate thread with the subject CPU 1214C - Want to connect a loop powered transmitter that outputs 4-20 mA, to the AI channel. Best regards |
Follow us on