3/8/2023 7:21 AM | |
Joined: 7/9/2015 Last visit: 10/4/2024 Posts: 3959 Rating: (590)
|
Hi, please try to reset S7-1200 to factory setting again - check steps in these FAQ: How can you delete the IP address and reset your S7-1200 to factory settings using the SIMATIC MC memory card?If this will not help, please contact Techical Support for SIMATIC. Regards, Towome |
|
|
This contribution was helpful to2 thankful Users |
3/8/2023 7:36 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289) |
Hi,
you can also try to perform a firmware update via SIMATIC Memory Card, even if the latest firmware version was already installed, it will be re-installed. It is worth a try. Firmware update for CPU 1214C, DC/DC/DC, 14DI/10DO/2AIregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
3/10/2023 7:15 AM | |
Joined: 7/9/2015 Last visit: 10/4/2024 Posts: 3959 Rating: (590)
|
Hi, this is the core data for the support - I think the solution depends on whether there is already one or whether it is being developed. What benefits are covered by basic support for products and systems from discrete manufacturing?Regards, Towome |
|
|
Follow us on