12/16/2013 1:16 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating:
|
perhaps you are interested in a keyboard which has not only capital letters? a standard model can be: Amazon.In the next days is christmas, perhaps you get some from |
Last edited by: Fafner at: 12/16/2013 1:17 PMBest Regards, |
|
12/17/2013 6:22 AM | |
Joined: 12/6/2007 Last visit: 6/26/2024 Posts: 12 Rating:
|
Dear Sir, which blocks using cpu to cpu communication though IWLAN? |
12/17/2013 9:17 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating:
|
Hey, the WLAN part of your network is 'transparent', which means you only have to project the AP and the Client in the right ways and then you can use every communication block you can use without WLAN. Obviously with a high network load, bad radio reception, multiple clients it can happen that you are getting delays in your communication. Perhaps have a look at CPU communication compendium and of course in the WLAN manuals. |
Best Regards, |
|
Follow us on